| Write / Read | About Source Ports | 
| Description | Sets and returns the ALC mode for the specified channel and port. Use GetSupportedALCModes to return a list of valid ALC modes for the VNA. | 
| VB Syntax | chan.ALCLevelingMode (sourcePort) = value | 
| Variable | (Type) - Description | 
| chan | (object) - A Channel object | 
| sourcePort | (long integer) - The source port for which to make this setting. If ports are remapped, specify the logical port number. Note: If the port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source VNA-x model, then you must use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port. | 
| value | (enum as naALCLevelingMode) - Choose from: 
 | 
| Return Type | Enum | 
| Default | naALCInternal | 
| Examples | chan.ALCLevelingMode(1) = 2 'Write | 
| C++ Syntax | HRESULT get_ALCLevelingMode(long port, tagNAALCLevelingMode* pVal); HRESULT put_ALCLevelingMode(long port,tagNAALCLevelingMode newVal); | 
| Interface | IChannel9 |