The following program is an example of setting up power uncertainty on a power meter.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as a <filename>.vbs file. Learn how to setup and run the macro.
PowerSensorCalFactorSegmentPMAR Object
PowerLossSegmentsPMAR_Collection
User Defined Power Meter Uncertainty File
Power Meter Uncertainty dialog description
Application Note (5988-9215EN)
| ' ' Keysight Technologies 2018 ' ' Uncertainty on power meter COM example ' ' This script execute and print the result of all the ' commands related to the uncertainty on power meter ' by using COM ''''''''''''''''''''''''''''''''''''''''' ' Create the Application object Dim app Set app = CreateObject("AgilentPNA835x.Application") ''''''''''''''''''''''''''''''''''''''''' 'Get the external devices dim externalDevices Set externalDevices = app.ExternalDevices ''''''''''''''''''''''''''''''''''''''''' ' Get the specific device in this example is Device2 dim myExternalDevice Set myExternalDevice = externalDevices.Item("Device2") ' print the selected external device type msgbox("External Device type:"& myExternalDevice.DeviceType) ''''''''''''''''''''''''''''''''''''''''' ' Get the External device extended propertiespecific ' dim PwrasRec Set PwrasRec =myExternalDevice.ExtendedProperties ' ' Get the uncertainty object ' dim PowerSensorUncertainty set PowerSensorUncertainty = PwrasRec.PowerSensorUncertainty ' ' Get the list of all the model available for uncertainty ' dim catalog catalog=PowerSensorUncertainty.UncertaintyModelCatalog ' ' Print the first element of the catalog ' msgbox("First Element of Power Meter with uncertainty catalog: "&catalog(1)) ' ' Get the selected uncertainty model Dim pwrmodel pwrmodel=PowerSensorUncertainty.UncertaintyModel ' print it msgbox("Selected Power Meter Model: "&pwrmodel) ' ' Get the custom uncertainty file ' If the model is not a CustomFile this will return Undefined as file name Dim pwruncfile pwruncfile=PowerSensorUncertainty.UncertaintyFile ' print it msgbox("Selected Power Meter Custom File: "&pwruncfile) ' ' Read the pwrmtr uncertainty value for a specific frequency and pwrlevel ' in this example 10GHz and 0.0 dBm Dim PwrMtrReadingUncertianty PwrMtrReadingUncertianty=PowerSensorUncertainty.PowerMtrReadingUncertainty(10e9,0.0) msgbox("10GHz and 0.0dBm nominal value Power Meter reading uncertainty variance: "&PwrMtrReadingUncertianty&" [W^2]") ' ' Read the power value which offer the best accuracy for the power meter Dim PowerForBestAcc PowerForBestAcc=PowerSensorUncertainty.PowerForBestAccuracy msgbox("Power Meter power for best accurary: "&PowerForBestAcc&" [dBm]") 
 |