Description | 
 Initializes a cable repeatability characterization for the specified channel and port.  | 
VB Syntax | 
 UncertChar.InitiateCableCharacterization (chan, port,iterations)  | 
Variable | 
(Type) - Description | 
| 
 UncertChar  | 
 A Characterizer (object)  | 
chan | 
 (Long) Channel number to calibrate. Note: chan MUST be the active channel.  | 
port | 
 (Long) Port number to use in the characterization.  | 
iterations | 
 (Long) Number of Iterative connections of the standards to be measured for the characterization.  | 
Return Type | 
 Not Applicable  | 
Default | 
 Not Applicable  | 
Examples | 
 oUncerChar.InitiateCableCharacterization(2,2,20)  | 
C++ Syntax | 
 HRESULT InitiateCableCharacterization([in] long channel, [in] long portNum, [in] long numIterationsPerStep, [out,retval] long* pNumSteps);  | 
Interface | 
 IUncertaintyCharacterizer  | 
The following existing commands on the GuidedCal object are used to perform the initialized cable repeatability characterization:
MinimumIterationsForStep Property
IterationCountForStep Property