Description |
Initializes a noise characterization for the specified channel and port. |
VB Syntax |
UncertChar.InitiateNoiseCharacterization (chan, firstPort, secondPort, iterations) |
Variable |
(Type) - Description |
UncertChar |
A Characterizer (object) |
chan |
(Long) Channel number to calibrate. Note: chan MUST be the active channel. |
firstPort |
(Long) First VNA port number on which the noise characterization is to be performed. |
secondPort |
(Long) Second VNA port number on which the noise characterization is to be performed. |
iterations |
(Long) Number of Iterative connections of the standards to be measured for the characterization. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
oUncerChar.InitiateNoiseCharacterization(2,1,2,20) |
C++ Syntax |
HRESULT InitiateNoiseCharacterization([in] long channel, [in] long firstPort, [in] long secondPort, [in] long numIterationsPerStep, [out,retval] long* pNumSteps); |
Interface |
IUncertaintyCharacterizer |
The following existing commands on the GuidedCal object are used to perform the initialized noise characterization:
MinimumIterationsForStep Property
IterationCountForStep Property