| Write/Read | About Mixer Configuration | 
| Description | When two LOs are used, sets or returns whether to select the sum or difference for the IF1 product. (Input + or - LO1 = IF1) 
 Note: There is also an IFSideband_Property on the Mixer Interface. | 
| VB Syntax | obj.IFSideband =value | 
| Variable | (Type) - Description | 
| obj | |
| value | (enum as ConverterSideBand) - Choose from: 0 or naLowSide Minus (-) on the Mixer setup dialog 1 or naHighSide Plus (+) on the Mixer setup dialog | 
| Return Type | Enum as ConverterSideBand | 
| Default | 0 - naLowSide | 
| Examples | conv.IFSideband = naLowSide | 
| C++ Syntax | HRESULT get_IFSideband(ConverterSideBand *pVal) HRESULT put_IFSideband(ConverterSideBand newVal) | 
| Interface | IConverter |