| Write/Read | About Power Leveling | 
| Description | Sets and returns the tone power leveling mode. | 
| VB Syntax | object.LevelingMethod = value | 
| Variable | (Type) - Description | 
| object | One of the following: | 
| value | (enum NAIMDLevelMethod) - Choose from: 0 - naNOLevel 1 - naLevelInput 2 - naEqualizeOutput 3 - naLevelOutput | 
| Return Type | Enum | 
| Default | naNOLevel | 
| Examples | imd.LevelingMethod = naEqualizeOutput 'Write | 
| levMode = ims.LevelingMethod 'Read | |
| C++ Syntax | HRESULT get_LevelingMethod(tagNALevelingMethods* pVal) HRESULT put_LevelingMethod(tagNALevelingMethods newVal) | 
| Interface | IIMSpectrum ISweptIMD |