Write/Read |
About CW Frequency |
Description |
Set the Continuous Wave (CW) frequency. Must first send chan.SweepType = naCWTimeSweep. See Also: calset.CWFrequency Property |
VB Syntax |
object.CWFrequency = value |
Variable |
(Type) - Description |
object |
One of the following: See also Measurement2 interface. |
value |
(double) CW frequency. Choose any number between: |
Return Type |
Double |
Default |
1e9 |
Examples |
chan.CWFrequency = 5e9 'Write |
cwfreq = chan.CWFrequency 'Read |
|
C++ Syntax |
HRESULT put_CWFrequency(double newVal) |
Interface |
IChannel IFOMRange |