Internal Second Source


The following VNA models include an internal second source.

Model

Total
# of Ports

PNA-X Opt 224

2

ALL PNA-X models

N522xA Opt 400's

4

How to use the second source

Benefits / Uses of the second source

Internal Second Source Restrictions

Source 1 and Source 2 are available at specific ports as follows:

4-port models

PNA-X  Opt 224 (PNA-X 2-port model):

Remotely Accessing the Internal Second Source

See Remotely Specifying a Source Port.