File | Instrument | Response | Stimulus | Utility | Cal | Apps | Remote ONLY
Frequency | Offset | Power | ALC | Recvr Lvl | Source Ports| # Points | Trigger :Ext | Auxiliary Trigger
Sweep settings:..Time | Setup | Segment | Power | Phase | Pulse Setup | DC Sources | Multi-Dimensional Sweep | Global Source
See Remotely Specifying a Source Port .
|
Description |
SCPI |
COM |
|---|---|---|
|
Start Freq |
||
|
Stop Freq |
||
|
Center Freq |
||
|
Span |
||
|
CW Frequency |
||
|
Number of Points |
||
|
Step size |
||
|
Freq Offset ON/Off |
||
|
Read available ranges |
||
|
Read number of ranges |
||
|
X-Axis display range |
||
|
Read range name |
||
|
Read range number |
||
|
Set range coupling |
||
|
Set sweep type |
||
|
Set CW freq |
||
|
Set start freq |
||
|
Set stop freq |
||
|
Set offset value |
||
|
Set divisor value |
||
|
Set multiplier value |
||
|
Freq. Offset Segment Sweep |
||
|
ON|OFF |
||
|
Add a segment |
||
|
Delete a segment |
||
|
Count the segments |
||
|
Center Frequency |
||
|
Frequency Span |
||
|
Start Frequency |
||
|
Stop Frequency |
||
|
Number of Points |
||
|
IF Bandwidth value |
||
|
IF Bandwidth control |
||
|
Source Power value |
||
|
Source Power control |
||
|
Sweep time value |
||
|
Sweep time control |
||
|
Test Set Switch |
||
|
Power Settings See Remotely Specifying a Source Port . |
||
|
Power ON | OFF |
||
|
Source Power (Auto | ON | OFF) |
||
|
Power Value |
||
|
Port Selection |
||
|
Couple Ports OFF | ON |
||
|
Attenuator Mode Auto|Manual |
||
|
Attenuation Value |
||
|
Power Slope ON | OFF |
||
|
Power Slope Value |
||
|
Receiver Attenuation |
||
|
Receiver Reference Attenuation |
None |
|
|
Receiver Test Attenuation |
None |
|
|
Shutdown or Restart System |
None |
|
|
See also Power Range remote commands |
||
|
Set power limit |
||
|
Set Calibration power limit |
None |
|
|
Power limit ON/OFF |
||
|
Power limit UI lock |
||
|
Set offset value |
||
|
Rx Level ON|OFF |
||
|
Select the reference receiver |
||
|
Sets all ports to pre-sweep or point leveling mode for the specified channel. |
None |
|
|
Enables or disables the receiver leveling maximum iteration search function. |
None |
|
|
Set maximum iterations |
||
|
Set tolerance |
||
|
Set offset value |
||
|
Separate IFBW |
||
|
Set Rx IFBW |
||
|
Safe mode ON|OFF |
||
|
Safe mode Max power |
||
|
Safe mode Min power |
||
|
Use Last Result for Source Power Cal |
||
|
Sets the specific PULSe4 behavior. |
None |
|
|
Sets all ports to pre-sweep or point leveling mode for the specified channel. |
None |
|
|
Enables or disables the receiver leveling maximum iteration search function. |
None |
|
|
Returns list of valid ALC Leveling Modes |
||
|
Set ALC Mode |
||
|
Specifying Source Ports See Remotely Specifying a Source Port. |
||
|
Returns the number of source ports. |
None |
|
|
Returns the string names of source ports. |
||
|
Returns the source port number of the specified string port name. |
None |
|
|
IF Bandwidth |
||
|
Previous IF Bandwidth |
None |
|
|
Next IFBandwidth |
None |
|
|
Reduce IF BW |
||
|
Sweep Time Value |
||
|
Returns the time the first point of a Time Sweep is measured. |
None |
|
|
Sets the time the analyzer takes to complete one sweep. |
None |
|
|
Number of Points |
||
|
Sweep Type (Lin | Pwr | CW | Seg | Phase) |
||
|
Sweep Generation (Stepped | Analog) |
||
|
Dwell Time Value |
||
|
Dwell Time Auto set the minimum dwell time |
||
|
Sweep Delay |
||
|
Alternate Sweeps |
||
|
External ALC |
||
|
Enable Point Sweep |
||
|
Fast Sweep |
||
|
Fast CW |
||
|
Set shift LO maximum frequency |
None |
|
|
Turn shift LO on or off |
None |
|
|
Returns whether or not the VNA has the low frequency extension (LFE) installed. |
||
|
Turns ON or OFF low frequency extension |
||
|
Start Power |
||
|
Stop Power |
||
|
Center |
||
|
Span |
||
|
ON|OFF |
||
|
Add a segment |
||
|
Delete a segment |
||
|
Delete all segments |
None |
|
|
Count the segments |
||
|
Read the segment number |
None |
|
|
Segment Center Frequency |
||
|
Segment Frequency Span |
||
|
Segment Start Frequency |
||
|
Segment Stop Frequency |
||
|
Number of Points |
||
|
IF Bandwidth |
||
|
IF Bandwidth Option |
||
|
IF Bandwidth Per Port |
||
|
Sweep Delay Time |
||
|
Sweep Dwell |
||
|
Sweep Mode |
||
|
Total Sweep Points |
||
|
Total Sweep Time |
None |
|
|
Source Power |
||
|
Source Power Option |
||
|
X-Axis Point Spacing |
||
|
Allow Arbitrary Segments |
||
|
Upload a segment table |
||
|
Download a segment table |
||
|
Sweep delay ON|OFF |
||
|
Sweep dwell ON|OFF |
||
|
IF Bandwidth resolution |
||
|
Sets or returns the SA data threshold |
||
|
Specifies whether SA Data Threshold can be set independently for each segment |
||
|
Sets or returns the SA multitone reference |
||
|
Specifies whether SA Reference Tone can be set independently for each segment |
||
|
Queries the maximum value of the SA Reference Tone |
None |
|
|
Queries the minimum value of the SA Reference Tone |
None |
|
|
Sets or returns the SA vector average |
||
|
Specifies whether SA Vector Averaging can be set independently for each segment |
||
|
Sets or returns the SA video bandwidth |
||
|
Sets or returns the noise figure bandwidth. |
||
|
Turns ON or OFF the noise figure bandwidth setting. |
||
|
Specifies whether SA Video Bandwidth can be set independently for each segment |
||
|
Phase Sweep type |
||
|
Set fixed phase value |
||
|
Phase sweep start value |
||
|
Phase sweep stop value |
||
|
Phase parameter |
||
|
Set Phase control mode |
||
|
Set reference port |
||
|
Read available phase control modes for the port |
||
|
Couple sweep settings |
||
|
Set number of sweep iterations |
||
|
Set sweep tolerance |
||
|
Set and read an array of phase offsets. |
||
|
Use phase offset array. |
||
|
Set and read an array of ratioed power offsets. |
||
|
Use power offset array. |
||
|
Set the fixed power ratioed value |
||
|
Set the start power ratioed value. |
||
|
Set the stop power ratioed value. |
||
|
Returns the available internal ports that the external port can be set to. |
None |
|
|
Sets and returns the internal port that the external port is routed through. |
None |
|
|
Returns the available phase control modes for the specified port. |
None |
|
|
Sets and returns the Phase Control mode. |
None |
|
|
Returns the available parameters. |
None |
|
|
Sets and returns the ratioed receivers (parameter) to use for phase control. |
None |
|
|
Returns the available ports that can be used as phase control reference ports for the phase controlled port. |
None |
|
|
Sets and returns the reference port for the Phase Control measurement. |
None |
|
|
Source (where trigger comes from) |
||
|
Source (Int | Ext | Manual) |
||
|
Internal | Manual |
None |
|
|
Trigger! (for Manual Source) |
||
|
Scope (what is triggered) |
||
|
Scope (Global | Channel) |
||
|
Channel Settings (how the channel responds to triggers) |
||
|
Continuous |
||
|
Read Continuous Mode |
None |
|
|
Number of Groups |
||
|
Read Groups |
None |
|
|
Hold |
||
|
Hold Mode (read-only) |
None |
|
|
All channels in Hold |
||
|
All channels Resume |
||
|
Single |
||
|
Trigger Mode |
||
|
Restart |
None |
|
|
Abort |
||
|
Scope (Global/Chan) |
||
|
Trigger Delay (Global) |
||
|
Trigger Delay (Channel) |
||
|
MeasTrigIn/ Hand I/O |
||
|
Level or Edge |
||
|
Neg/Low or Pos/High |
||
|
Accept Trigger Before Armed |
||
|
Ready for Trigger Indicator (Out) |
||
|
MeasTrig Rdy/ Hand I/O |
CONTrol:SIGNal:STReamline:RTRigger[:STATe] CONTrol:SIGNal:PXI:RTRigger[:STATe] |
None |
|
Checks if the PNA is ready for a hardware trigger |
||
|
High / Low |
||
|
Which AuxTrig connector pair being used. |
N/A |
|
|
How many Aux connector pairs. |
||
|
AUX TRIG OUT |
||
|
Enable |
||
|
Global or Channel Pref. |
||
|
Polarity (Pos/Neg) |
||
|
Position (Before/After acq) |
||
|
OUT Pulse width |
||
|
Point or Sweep. |
||
|
Rear SMB |
||
|
Backplane |
||
|
AUX TRIG (Ready) IN |
||
|
Enable Handshake |
||
|
Edge or Level Level NOT in UI. |
||
|
Polarity High/leading or Low/trailing. |
||
|
Delay |
||
|
Pulse Meas Mode |
||
|
Autodetect Pulse mode |
||
|
Set Pulse Mode (Narrow | Wide) |
||
|
Autoselect IFBW |
||
|
Autoselect IF Gain |
None |
|
|
Autoselect Pulse clock period |
||
|
Autoselect Width and Delay |
||
|
Autoselect Pulse Gens |
||
|
Autoselect CW Sweep Time |
||
|
Pulse (manual) Settings |
||
|
Set master pulse frequency |
||
|
Set master pulse period |
||
|
Set master pulse width |
||
|
Set pulse start time |
||
|
Set pulse stop time |
|
Enable Pulse output ON | OFF |
||
|
Set Pulse Period for ALL pulse generators |
||
|
Set Pulse Delay |
||
|
Set Pulse Width |
||
|
Set Pulse delay increment |
||
|
Enables Subpoint triggering |
||
|
Set Pulse Invert |
||
|
Internal Pulse Modulator Enable |
||
|
Returns the ADC delay. |
||
|
Sets the time lag between the pulse drive signal and the actual RF output. |
||
|
Enables / Disables offset delays. |
||
|
Sets and reads the device being controlled by the pulse generator output. |
||
|
Enable pulse4 to monitor ADC activity. |
||
|
Sets the specific PULSe4 behavior. |
None |
|
|
PulseSyncIn Trigger Polarity |
||
|
PulseSyncIn Trigger Type |
||
|
Sync receiver to Pulse0 (enable pulse0) |
||
|
Pulse Trigger Source |
||
|
Source names catalog |
||
|
Enable source outputs |
||
|
Source state |
||
|
Start DC |
||
|
Stop DC |
||
|
Data |
||
|
Set and return the Max DC limit value for a DC source |
||
|
Set and return the Min DC limit value for a DC source |
|
Set and read the order for the specified DC source in the multi-dimensional sweep. |
SOURce:DC:DIMension:ORDer |
|
|
Set and read the specified DC source’s ON/OFF state in the multi-dimensional sweep. |
SOURce:DC:DIMension[:STATe] |
|
|
Read the names of source domains in the multi-dimensional sweep whose state is ON and whose dimension order is the specified dimension order. |
SOURce:DIMension:CATalog? |
|
|
Read the highest dimension order in the multi-dimensional sweep. |
SOURce:DIMension:COUNt? |
|
|
Set and read the point count for the specified dimension order in the multi-dimensional sweep. |
SOURce:DIMension:POINts |
|
|
Set and read the repeat count for the specified dimension order in the multi-dimensional sweep. |
SOURce:DIMension:REPeat:COUNt |
|
|
Set and read the source frequency domain’s order in the multi-dimensional sweep. |
SOURce:FREQuency:DIMension:ORDer |
|
|
Set and read the source frequency domain’s ON/OFF state in the multi-dimensional sweep. |
SOURce:FREQuency:DIMension[:STATe] |
|
|
Set and read the fixed frequency value for a specific port. |
SOURce:FREQuency:FIXed |
|
|
Set and read the start frequency value for a specific port. |
SOURce:FREQuency:STARt |
|
|
Set and read the stop frequency value for a specific port. |
SOURce:FREQuency:STOP |
|
|
Set and read the source phase domain’s order in the multi-dimensional sweep. |
SOURce:PHASe:DIMension:ORDer |
|
|
Set and read the source phase domain’s ON/OFF state in the multi-dimensional sweep. |
SOURce:PHASe:DIMension[:STATe] |
|
|
Set and read the source power domain’s order in the multi-dimensional sweep. |
SOURce:POWer:DIMension:ORDer |
|
|
Set and read the source power domain’s ON/OFF state in the multi-dimensional sweep. |
SOURce:POWer:DIMension[:STATe] |
|
|
Set and return the frequency of the specified global source. |
None |
|
|
Set and return the output state of the specified global source. |
None |
|
|
Set and return the global sources that ignore the power off setting. |
None |
|
|
Set and return the power of the specified global source. |
None |
|
|
Set and return the global state of the specified global source. |
None |
|
|
Loads the internal source modulation file. |
None |
|
|
Returns the name of the currently loaded internal source modulation file. |
None |
|
|
Set and return the state of the specified internal source modulation port. |
None |
|
![]()