Control Commands


Specifies the settings to remotely control the rear panel connectors, an external test set, Calpod modules, and ECal Module state.

CONTrol

AUXiliary - More Commands

CALPod:COMMand

CHANnel:INTerface:CONTrol

     | CONFig:RECall

     | [STATe]

ECAL:MODule

     | PATH

          | COUNt?

          | STATe

     | PORT

          | CATalog

          | STATe

               | CATalog

               | [:SELect]

     | STATe

EXTernal:TESTset - More Commands

HANDler - More Commands

NOISe:SOURce[:STATe]

PHASe

     | COUNt?

     | MODule

          | DATA

          | STORe

          | MODel?

          | SERial?

          | SETup

SIGNal:

     | TRIGger

          | ATBA

          | OUTP

     | AIO

| PIN

          | COUNt?

          | FUNCtion

               | CATalog?

 | INPut:LEVel?

 | CHANnel

 |FUNCtion

 | CATalog

    | KDMI

          | MAIN

                | COUNt?

                | CHANnl:FUNCion

                | FUNCtion 

                    | CATalog?

                | INPut:LEVel?

| LOGic

          | SUB

               | COUNt?

               | CHANnl:FUNCion

               | FUNCtion

                     | CATalog?

                | INPut:LEVel?

| LOGic

| PXI

| RTRigger

 | [:STATe]

 | ROUTe

| TRIGger

 | OUTPut

| [:STATe]

| ROUTe

| STReamline

| RTRigger

 | [:STATe]

 | ROUTe

| TRIGger

 | OUTPut

| [:STATe]

| ROUTe

Click on a keyword to view the command details.

Blue command is superseded.

See Also


CONTrol:CALPod:COMMand <string>

Applicable Models: N522xB, N523xB, N524xB, M937xA, E5080A/B, E5081A, P937xA, P50xxA/B, M980xA, M983xA

(Write-Read)  Sends commands that control a Calpod module. Reads query versions Calpod commands.

See ALL Calpod commands.

Learn more about Calpod.

Parameters

 

<string>

Calpod command. See ALL Calpod commands that can be used in this string.

Write Example

CONT:CALP:COMM 'CALP:INIT:ACT'

'Enclose all strings in SINGLE quotes (NOT double quotes)

Query Syntax

CONTrol:CALPod:COMMand? <string>

Relevant only for query strings.

Read Example

CONT:CALP:COMM? '*OPC?'

'returns 0 if the calpod software is currently processing an operation

'returns 1 if operations are complete

Return Type

String

Default

Not Applicable


CONTrol:CHANnel:INTerface:CONTrol:CONFig:RECall[:STATe] <string>

Applicable Models: N522xB, N523xB, N524xB, E5080A

(Write-only)  Recalls an Interface Control configuration file.  Learn more about Interface Control.

Parameters

 

<string>

File name and extension (.xml) of the configuration file to recall. Files are typically stored in the default folder "D:\". To recall from a different folder, specify the full path name.

Examples

CONT:CHAN:INT:CONT:CONF:REC 'MyConfigFile.xml'

control:channel:interface:control:config:recall:state 'D:\MyFile.xml'

Query Syntax

Not Applicable

Default

Not Applicable


CONTrol:CHANnel:INTerface:CONTrol[:STATe] <bool>

Applicable Models: N522xB, N523xB, N524xB, E5080A/B, E5081A

(Read-Write)  Enables and disables ALL Interface Control settings. To send data, the individual interfaces must also be enabled. Learn more about Interface Control.

Parameters

 

<bool>

Boolean

OFF (0) - Interface Control is disabled;NO control data is sent.

ON (1) - Interface Control is enabled.

Examples

CONT:CHAN:INT:CONT 1

control:channel:interface:control:state 0

Query Syntax

CONTrol:CHANnel:INTerface:CONTrol[:STATe]?

Return Type

Boolean

Default

OFF (0)


CONTrol:ECAL:MODule<num>:PATH:COUNt? <name> Superseded

Applicable Models: All

This command is replaced with CONTrol:ECAL:MODule:PORT:CATalog?

(Read-only)  Returns the number of unique states that exist for the specified path name on the selected ECal module.

This command performs exactly the same function as SENS:CORR:CKIT:ECAL:PATH:COUNt?

Use the CONT:ECAL:MOD:PATH:STAT command to set the module into one of those states.  

Use SENS:CORR:CKIT:ECAL:PATH:DATA? to read the data for a state.

 

Parameters

 

[num]

Optional argument. USB number of the ECal module.  If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities.

<name>

Name of the path for which to read number of states.  Choose from:

Reflection paths

  • A

  • B

  • C (4-port modules)

  • D (4-port modules)

Transmission paths

  • AB

  • AC (4-port modules)

  • AD (4-port modules)

  • BC (4-port modules)

  • BD (4-port modules)

  • CD (4-port modules)

Note: For each transmission path, the first of the available states is the through state, the second is the confidence (attenuator) state.

Examples

CONT:ECAL:MOD:PATH:COUNt? A

control:ecal:module2:path:count? cd

See example program

Return Type

Integer

Default

Not Applicable


CONTrol:ECAL:MODule<num>:PATH:STATe <path>, <stateNum> Superseded

Applicable Models: All

This command is replaced with CONTrol:ECAL:MODule:PORT:STATe[:SELect]

(Write-only) Sets the internal state of the selected ECAL module. This command supersedes CONT:ECAL:MOD:STAT.

Parameters

 

[num]

Optional argument. USB number of the ECal module.  If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities.

<path>

Path name for which to set a state.  

Note: The impedance paths are not independent. For example, changing the impedance presented on path A will cause a change to the impedance on path B.

Choose from:

Reflection paths

  • A

  • B

  • C (4-port modules)

  • D (4-port modules)

Transmission paths

  • AB

  • AC (4-port modules)

  • AD (4-port modules)

  • BC (4-port modules)

  • BD (4-port modules)

  • CD (4-port modules)

<stateNum>

Number of the state to set. Refer to the following table to associate the <stateNum> with a state in your ECal module.

In addition, CONT:ECAL:MOD:PATH:COUNt? returns the number of states in the specified ECal module.

<stateNum>

N4432x and
N4433x States

N4431x States

N469x and N755x States**

8509x States

One-Port Reflection States

1

Open

Open

Impedance 1

Open

2

Short

Short

Impedance 2

Short

3

Impedance 1

Impedance 1

Impedance 3

Impedance 1

4

Impedance 2

Impedance 2

Impedance 4

Impedance 2

5

 

 

Impedance 5

 

6

 

 

Impedance 6

 

7

 

 

Impedance 7

 

Two-Port Transmission States

1

Thru

Thru

Thru

Thru

2

Confidence

Confidence

Confidence

Confidence

** The following modules have only FOUR Impedance states (1, 2, 3, 4): N4690B ,N4691B ,N4692A ,N4696B, N7550A - N7556A.

Examples

CONT:ECAL:MOD:PATH:STATe A,5

control:ecal:module2:state BC,1

See example program

Query Syntax

Not Applicable

Default

Not Applicable


CONTrol:ECAL:MODule<num>:PORT:CATalog?

Applicable Models: All

(Read-only)  Returns the list of port labels on the selected ECal module.

Parameters

 

[num]

Optional argument. USB number of the ECal module.  If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities.

Examples

CONT:ECAL:MOD2:PORT:CAT?

> “A,B,C,D” // 4-port ECal

> “1-A,1-B,1-C,1-D,1-E,1-F,2-A,2-B,…,6-E,6-F” // 6-module of N756xA (36-port ECal)

Return Type

Character

Default

Not Applicable


CONTrol:ECAL:MODule<num>:PORT:STATe:CATalog? <type>,<port>

Applicable Models: All

(Read-only)  Returns  a list of state or port labels for ECal. The returned values is used for CONTrol:ECAL:MODule:PORT:STATe[:SELect]

Parameters

 

[num]

Optional argument. USB number of the ECal module.  If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities.

<type>

Choose from:

  • REFL :Reflection

  • TRAN :Transmission

  • CONF:  Confidence

<port>

Port label. Candidates are response of the CONT:ECAL:MOD:PORT:CAT? command.

Response: Depends on the <type> value.

  • If <type> is REFL, This command returns one port state number. (Ex. 1=Open, 2=Short, etc.)
  • If <type> is TRAN or CONF,This command returns candidate port labels that are possible to connect to.

Examples

CONT:ECAL:MOD2:PORT:STAT:CAT? REFL,’A’

> “1,2,3,4” // 4-state ECal module

> “1,2,3,4,5,6,7” // 7-state ECal module

CONT:ECAL:MOD2:PORT:STAT:CAT? TRAN,’A’

> “B,C,D” // Port ‘A’ can be connected to B, C or D

CONT:ECAL:MOD128:PORT:STAT:CAT? TRAN,’2-A’

> “1-F,2-B,2-F” // N756xA example

Return Type

Numeric

Default

Not Applicable


CONTrol:ECAL:MODule<num>:PORT:STATe[:SELect] <type>,<port>,<stateOrPort>

Applicable Models: All

(Write-only)  Sets the internal state of the ECal module.

Parameters

 

[num]

Optional argument. USB number of the ECal module.  If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities.

<type>

Choose from:

  • REFL :Reflection

  • TRAN :Transmission

  • CONF:  Confidence

<port>

Port label. Candidates are response of the CONT:ECAL:MOD:PORT:CAT? command.

Response: Depends on the <type> value.

  • If <type> is REFL, This command returns one port state number. (Ex. 1=Open, 2=Short, etc.)
  • If <type> is TRAN or CONF,This command returns candidate port labels that are possible to connect to.

<stateOrPort>

State or port label. The CONT:ECAL:MOD:PORT:STAT:CAT? command returns possible parameter.

Examples

CONT:ECAL:MOD2:PORT:STAT:SEL REFL,’A’,’2’

CONT:ECAL:MOD128:PORT:STAT:SEL REFL,’1-C’,’6’

CONT:ECAL:MOD2:PORT:STAT:SEL TRAN,’A’,’C’

CONT:ECAL:MOD128:PORT:STAT:SEL TRAN,’2-A’,’1-F’

Return Type

Not Applicable

Default

Not Applicable


CONTrol:ECAL:MODule<num>:STATe <value> Superseded

Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA

This command is replaced with  CONT:ECAL:MOD:PATH:STATe.

(Write-only) Sets the internal state of the selected ECAL module.

Parameters

 

[num]

Optional argument. USB number of the ECal module.  If unspecified (only one ECal module is connected to the USB), <num> is set to 1.  If two or more modules are connected, use SENS:CORR:COLL:CKIT:INF? to verify their identity.

<value>

Integer code for switching the module. The following are codes for Keysight ECal modules.

8509x Modules

State

Port A

Port B

Open

0

0

Short

43

43

Load

33

33

Mismatch

4

16

Thru

84

Confidence

20

 

N469xA/B and N755x Modules (See also, N469xD Modules)

State

Port A

Port B

Open

36

33

Short

39

45

Load

37

37

Mismatch
(Offset short)

53

53

Impedance 5
(Offset open)

5

5

Impedance 6
(Offset short)

21

21

Impedance 7
(Offset short)

38

41

Thru

42

Confidence

40

N469xD Modules (See also, N469xA/B and N755x Modules)

State

Port A

Port B

Open

9

3

Short

15

27

Load

11

11

Mismatch
(Offset short)

43

43

Impedance 5
(Offset open)

10

10

Impedance 6
(Offset short)

42

42

Impedance 7
(Offset short)

13

19

Thru

21

Confidence

17

 

N4431A Modules

State

Port A

Port B

Port C

Port D

Open

-1398

-1384

-2774

-2654

Short

-1350

-1381

-2582

-2642

Load

26985

-26986

-26986

26985

Mismatch

-26986

26985

26985

-26986

Path

Thru

Confidence

AB Path

-2590

-598

AC Path

-4011

85

AD Path

-2517

16042

BC Path

-1650

-598

BD Path

-4011

85

CD Path

-1352

16042

 

N4432A and N4433A Modules

State

Port A

Port B

Port C

Port D

Open

-6971

-11835

-14895

-14876

Short

-14395

-12859

-14899

-14905

Load

-14907

-14907

-14907

-14907

Offset Short

-9787

-6459

-14874

-14887

Path

Thru

Confidence

AB Path

13765

30069

AC Path

-10519

-2327

AD Path

-10538

-2346

BC Path

-5655

-1559

BD Path

-5674

-1578

CD Path

-15051

30069

Examples

CONT:ECAL:MOD:STAT 36
control:ecal:module2:state 38

Query Syntax

Not Applicable

Default

Not Applicable


CONTrol:MULTiplexer<id>:OUTPut:<grp>[:DATA] <num>

Applicable Models: E5080A/B, E5081A

(Read-Write) Sets or returns the output port data for specified group with id of the E5092A multiport test set.

Notes: This command is available only for E5092A multiport test set.

Parameters

 

<id>

Id of the multiport test set either 1 or 2. If unspecified, Id is assumed to be 1.

<grp>

A | B | C | D

<num>

An integer specifying the decimal value of the control line. Values are obtained by adding weights from the following table that correspond to individual lines.

The output port data range is between 0 to 255 (0=All line are turns OFF and 255 all lines are turn ON).

Line

Weight

1

1

2

2

3

4

4

8

5

16

6

32

7

64

8

128

Examples

CONT:MULT1:OUTP:B 8

Query Syntax

CONTrol:MULTiplexer<id>:OUTPut:<grp>[:DATa]?

Return Type

Numeric

Default

0


CONTrol:MULTiplexer<id>:OUTPut:<grp>VOLTage[:DATA] <volt>

Applicable Models: E5080A/B, E5081A

(Read-Write) Sets or returns the output voltage for specified group with id of the E5092A multiport test set.

Notes: This command is available only for E5092A multiport test set.

Parameters

 

<id>

Id of the multiport test set either 1 or 2. If unspecified, Id is assumed to be 1.

<grp>

A | B | C | D

<volt>

Output voltage range for <grp> is between 0 to 5.2V and resolution is 10mV.

Examples

CONT:MULT1:OUTP:B:VOLT 4.2

Query Syntax

CONTrol:MULTiplexer<id>:OUTPut:<grp>:VOLtage[:DATa]?

Return Type

Numeric

Default

0 V

CONTrol:NOISe:SOURce[:STATe] <bool>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write)  Set and read the noise source (28V) ON and OFF.

Parameters

 

<bool>

Boolean

OFF (0) - Noise Source OFF

ON (1) - Noise Source ON

Examples

CONT:NOIS:SOUR 1

control:noise:source:state 0

Query Syntax

CONTrol:NOISe:SOURce[:STATe]?

Return Type

Boolean

Default

For VNA models with a Noise Figure option (028/029/H29), the 28V line is ON at application start and after a preset.  The ON/OFF state is also available from a VNA softkey menu.

For VNA models WITHOUT a Noise Figure option (028/029/H29), the 28V line is OFF at application start and its state is not affected by a preset. The ON/OFF state is NOT available from a VNA softkey menu.


CONTrol:PHASe:COUNt?

Applicable Models: All

(Read only) Reads the number of phase reference modules connected.

Parameters

None

Examples

CONT:PHAS:COUN?

control:phase:count?

Return Type

Numeric value

Default

N/A


CONTrol:PHASe:MODule[x]:DATA:STORe <path>

Applicable Models:  All

(Write-only) Reads the calibration data from the phase reference of the specified module (x), and writes the data to the Path

Parameters

 

<path>

(String) Directory path to stored data.

Examples

CONT:PHAS:MOD1:DATA:STOR "D:MyPhaseRefCalData.csv"

control:phase:module1:data:store "D:MyPhaseRefCalData.csv"

Return Type

N/A

Default

N/A


CONTrol:PHASe:MODule[x]:MODel?

Applicable Models:  All

(Read only) Reads the model number of the specified module (x).

Parameters

None

Examples

CONT:PHAS:MOD1:MOD?

control:phase:module1:model?

Return Type

String

Default

N/A


CONTrol:PHASe:MODule[x]:SERial?

Applicable Models:  All

(Read only) Reads the serial number of the specified module (x).

Parameters

 

Examples

CONT:PHAS:MOD1:SER?

control:phase:module1:serial?

Return Type

Numeric

Default

N/A


CONTrol:PHASe:MODule[x]:SETup <divideNumber>

Applicable Models: All

(Write-only) Turns on the phase reference, and sets the divide number.

Parameters

 

<divideNumber>

Divide number can be 1, 2, 4, 8, 16.

Examples

CONT:PHAS:MOD1:SET 2

control:phase:module1:setup 2

Return Type

Numeric

Default

N/A


CONTrol:SIGNal <conn>,<char>   

Applicable Models: N522xB, N523xB, N524xB

(Read-Write)  Configures external triggering in the VNA.

Note: To configure external triggering in the current VNA models, use the Trigger commands.

Parameters

 

<conn>

Rear Panel connector to send or receive trigger signals. Choose from:

BNC1  Trigger IN from rear-panel Trigger IN BNC connector

Note: Only one of the input connectors is active at a time. When a command is sent to one, the VNA automatically makes the other INACTIVE.

BNC2  Trigger OUT to rear-panel Trigger OUT BNC connector.

MATHtrigger - Trigger IN from rear-panel Material Handler connector Pin 18

RDY - Ready for trigger OUT.

<char>

INACTIVE - Disables the specified connector <conn>.

Choose from ONLY the following when <conn> is set to BNC1 or AUXT or MATHtrigger:

  • TIENEGATIVE - (Trigger In Edge Negative) - Triggers the VNA when receiving a negative going signal

  • TIEPOSITIVE - (Trigger In Edge Positive) - Triggers the VNA when receiving a positive going signal

  • TILLOW - (Trigger In Level Low) - Triggers the VNA when receiving a low level signal

  • TILHIGH - (Trigger In Level High) - Triggers the VNA when receiving a High-level signal

Choose from ONLY the following when <conn> is set to BNC2:

Use CONTrol:SIGNal:TRIGger:OUTP to enable the BNC2 output.

The following selections send a positive or negative pulse before or after each trigger acquisition. This normally occurs each sweep unless a channel is in point trigger mode.

  • TOPPAFTER - (Trigger Out Pulse Positive After) - Sends a POSITIVE going TTL pulse at the END of each trigger acquisition.

  • TOPPBEFORE - (Trigger Out Pulse Positive Before) - Sends a POSITIVE going TTL pulse at the START of each trigger acquisition.

  • TOPNAFTER - (Trigger Out Pulse Negative After) - Sends a NEGATIVE going TTL pulse at the END of each trigger acquisition.

  • TOPNBEFORE - (Trigger Out Pulse Negative Before) - Sends a NEGATIVE going TTL pulse at the START of each trigger acquisition.

Choose from ONLY the following when <conn> is set to RDY:

  • LOW   Outputs a TTL low when the VNA is ready for trigger. (Default setting)

  • HIGH  Outputs a TTL high when the VNA is ready for trigger.

Examples

CONT:SIGN BNC1,TIENEGATIVE
control:signal bnc2,toppbefore

CONT:SIGN RDY,LOW

Query Syntax

CONTrol:SIGNal? <conn>

In addition to the arguments listed above, the following is also a possible returned value:

NAVAILABLE - This feature is not available on this VNA

Return Type

Character

Default

At Preset:

BNC1 = INACTIVE
BNC2 = INACTIVE
AUXT = TILHIGH

When Output is enabled:

BNC1 = INACTIVE
BNC2 = TOPPAFTER
AUXT = TILHIGH


CONTrol:SIGNal:TRIGger:ATBA <bool>

Applicable Models: N522xB, N523xB, N524xB. M980xA, P50xxA/B, P93xxB, E5080B, E5081A

(Read-Write)  Accept Trigger Before Armed  Determines what happens to an EDGE trigger signal if it occurs before the VNA is ready to be triggered. (LEVEL trigger signals are always ignored.)  For more information, see External triggering.

Parameters

 

<bool>

Boolean

OFF (0) - A trigger signal is ignored if it occurs before the VNA is ready to be triggered.

ON (1) - A trigger signal is remembered and then used when the VNA becomes armed (ready to be triggered). The VNA remembers only one trigger signal.

Examples

CONT:SIGN:TRIG:ATBA 0
control:signal:trigger:atba ON

Query Syntax

CONTrol:SIGNal:TRIGger:ATBA?

Return Type

Boolean

Default

OFF


CONTrol:SIGNal:TRIGger:OUTP <bool>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write)  Output Enabled  The VNA can be enabled to send trigger signals out the rear-panel TRIGGER OUT BNC connector. Use CONTrol:SIGNal to configure for output triggers.

Note: To configure external triggering in the current VNA models, use the Trigger commands.

For more information, see External triggering.

Parameters

 

<bool>

Boolean

OFF (0) - VNA does NOT output trigger signals.

ON (1) - VNA DOES output trigger signals.

Examples

CONT:SIGN:TRIG:OUTP 1

control:signal:trigger:outp OFF

Query Syntax

CONTrol:SIGNal:TRIGger:OUTP?

Return Type

Boolean

Default

OFF


CONTrol:SIGNal:AIO:PIN:COUNt?

Applicable Models: E5080B, E5081A

(Read only) Read the total number of pin on the application I/O. In case for the E5080B, always 15. For more information, see application I/O.

Parameters

None

Examples

CONT:SIGN:AIO:PIN:COUN?

control:signal:aio:pin:count?

Query Syntax

CONTrol:SIGNal:AIO:PIN:COUNt?

Return Type

Numeric value

Default

15


CONTrol:SIGNal:AIO:PIN<pin>:FUNCtion <func>

Applicable Models: E5080B, E5081A

(Write-Read) Set and Read the function for the specified port in the application I/O interface. The assigned settings are not saved in a state file, but the setting is stored when changing function and recall them at the next firmware start up.

Parameters

 

<pin>

Pin Number.

<func>

function name

Function name

Description

Type

Assignable

pot number

Default

Assignment

PULSE_OUT1

1st pulse output

Output

10

10

PULSE_OUT2

2nd pulse output

Output

11

11

PULSE_OUT3

3rd pulse output

Output

12

12

PULSE_OUT4

4th pulse output

Output

13

13

RF_PULSE_MOD_IN

RF pulse modulation

Input

8

8

PULSE_SYNC_IN

Pulse generator synchronization trigger input

INPUT

7

7

AUX TRIG IN

AUX trigger input

INPUT

7

N/A

INPUT

Arbitrary input (CONT:SIGN:APPL:INP:LEV? to query the level on the assigned port)

Input

1 to 5, 10 to 13

N/A

LOW

Set the Low (Output Low level) at the assigned port.

Output

1 to 5, 10 to 13

1 to 5

HIGH

Set the High (Output High level) at the assigned port

Output

1 to 5, 10 to 13

N/A

NF_SOURCEx (x=1,2,...) *1

Noise Figure source switch control for port x

Output

1 to 5, 10 to 13

N/A

NF_RECEIVERx (x=1,2,...) *1

Noise Figure receiver switch control for port x

Output

1 to 5, 10 to 13

N/A

DCV_ON

+12V power output enable

Output

14

N/A

DCV_OFF

+12V power output disable

Output

14

14

CHANNEL_CTRL

Function is controlled per channel by :CONTrol:SIGNal:AIO:PIN<pin>:CHANnel<ch>:FUNCtion

 

1 to 5, 10 to 13

N/A

*1) For Noise Figure switch control, the signal is asserted no matter which pins are used in the NF channel if the port index(x) is not specified.

Examples

CONT:SIGN:AIO:PIN:FUNC "LOW"

control:signal:aio5:pin:function "NF_SOURCE15"

Query Syntax

CONTrol:SIGNal:AIO:PIN:FUNC?

Return Type

<sting>

Default

See the table in <func>


CONTrol:SIGNal:AIO:PIN<pin>:FUNCtion:CATalog?

Applicable Models: E5080B, E5081A

(Read Only) Read the list of the available function for the specified pin in the application I/O. Example, "RF_PULSE_MOD_IN" is returned for the pin 8.

Parameters

 

<pin>

Pin Number.

Examples

CONT:SIGN:AIO:PIN3:FUNC:CAT?

control:signal:aio:pin3:function:catalog?

Query Syntax

CONTrol:SIGNal:AIO:PIN:FUNC:CAT?

Return Type

<sting>, available function list with Comma separated chars

Default

See the table in <func> of  CONTrol:SIGNal:APPLication:FUNC?


:CONTrol:SIGNal:AIO:PIN<pin>:CHANnel<ch>:FUNCtion <func>

Applicable Models: E5080B, E5081A

(Write-Read) Set and read the function for the selected pin on the Application I/O connector. It is set on channel basis and reflected only when “CHANNEL_CTRL” is selected in :CONTrol:SIGNal:AIO:PIN<pin>:FUNCtion <func> for the specified pin. The setting is saved in the state file and subject to preset. Function can be selected from Output signals

Parameters

 

<pin>

Pin Number 1-5, 10-13

<ch>

Channel number

Examples

:CONT:SIGN:AIO:PIN3:CHAN1:FUNC?

:CONT:SIGN:AIO:PIN3:CHAN1:FUNC “HIGH”

Query Syntax

CONTrol:SIGNal:AIO:PIN:CHAN:FUNC?

Return Type

<char>

Default

HIGH


:CONTrol:SIGNal:AIO:PIN<pin>:CHANnel<ch>:FUNCtion:CATalog

Applicable Models: E5080B, E5081A

(Read Only) Read the catalog of the functions assignable to the pin on the Application I/O connector.

Parameters

 

<pin>

Pin Number 1-5, 10-13

Examples

:CONT:SIGN:AIO:PIN5:CHAN1:FUNC:CAT?

control:signal:aio:pin5:channel:function:catalog?

Query Syntax

CONTrol:SIGNal:AIO:PIN:CHAN:FUNC:CAT?

Return Type

Comma separated chars

Default

NA


CONTrol:SIGNal:AIO:PIN<pin>:INPut:LEVel?

Applicable Models:  E5080B, E5081A

(Read only) Read the level of the specified INPUT pin of the application I/O. This command reads the level immediately after its execution. It is not necessary to assign the pin as INPUT by command.  When the specified pin number is 6 to 9 or 14, "Specified Application IO port is not input port." error is returned.

Parameters

 

<pin>

Pin Number. (E5080B: 1 to 5, 10 to 13)

Examples

CONT:SIGN:AIO:PIN:INP2:LEV?

control:signal:aio:pin:input1:level?

Query Syntax

CONTrol:SIGNal:AIO:PIN:INPut:LEVel?

Return Type

Char ("HIGH" or "LOW")

Default

N/A


CONTrol:SIGNal:KDMI:MAIN:COUNt?

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Read only) Read the number of ports in the main control port of the I/O connector interface.  In case for the M980xA/P50xxA, always 6.

For more information, see I/O Connector Interface (M980xA/P50xxA)

Parameters

None

Examples

CONT:SIGN:KDMI:MAIN:COUN?

control:signal:kdmi:main:count?

Query Syntax

CONTrol:SIGNal:KDMI:MAIN:COUNt?

Return Type

Numeric value

Default

6.


CONTrol:SIGNal:KDMI:MAIN<port>:CHANnel<ch>:FUNCtion <func>

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Write-Read) Set and Read the function for the specified port and channel in the main of the I/O adapter interface.  To use this, set CONTrol:SIGNal:KDMI:MAIN:FUNCion at CHANNEL_CTRL. The setting is saved in the state file and subject to preset. Function can be selected from Output signal.

Parameters

 

<port>

Port Number. The number of total ports is returned by CONTrol:SIGNal:KDMI:MAIN:COUNt?.

<func>

function name

Function name

Description

Type

Assignable pot number

PULSE_OUT1

1st pulse output

Output

1

PULSE_OUT2

2nd pulse output

Output

2

PULSE_OUT3

3rd pulse output

Output

3

PULSE_OUT4

4th pulse output

Output

4

LOW

Set the Low (Output Low level) at the assigned port.

Output

1, 2, 3 or 4

HIGH

Set the High (Output High level) at the assigned port

Output

1, 2, 3 or 4

NF_SOURCEx (x=1,2,...) *1

Noise Figure source switch control for port x

Ouptpu

1, 2, 3 or 4

NF_RECEIVERx (x=1,2,...) *1

Noise Figure receiver switch control for port x

Output

1, 2, 3 or 4

NF_LOy (y=1,2,…)

Noise Figure LO switch control for module y

Output

1, 2, 3 or 4

*1) For Noise Figure switch control, the signal is asserted no matter which ports are used in the NF channel if the port/module index(x) is not specified.

Examples

CONTrol:SIGNal:KDMI:MAIN1:FUNCion "CHANNEL_CTRL"

CONT:SIGN:KDMI:MAIN1:CHAN1:FUNC "LOW"

 

CONTrol:SIGNal:KDMI:main2:FUNCion "CHANNEL_CTRL"

control:signal:kdmi:main2:channel2:function "NF_LO1"

Query Syntax

CONTrol:SIGNal:KDMI:MAIN:CHAN:FUNC?

Return Type

<sting>

Default

HIGH


CONTrol:SIGNal:KDMI:MAIN<port>:FUNCtion <func>

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Write-Read) Set and Read the function for the specified port in the main c of the I/O adapter interface.  The assigned settings are preserved for each system configuration even after preset, firmware restart and power on/off.   The CONTrol:SIGNal:KDMI:MAIN:CHANnel:FUNCion allows you to set the function independently for each channel.

For more information, see I/O Connector Interface

Parameters

 

<port>

Port Number. The number of total ports is returned by CONTrol:SIGNal:KDMI:MAIN:COUNt?.

<func>

function name

Function name

Description

Type

Assignable pot number

PULSE_OUT1

1st pulse output

Output

1

PULSE_OUT2

2nd pulse output

Output

2

PULSE_OUT3

3rd pulse output

Output

3

PULSE_OUT4

4th pulse output

Output

4

RF_PULSE_MOD_IN

RF pulse modulation

Input

5 (Factory default)

INPUT

Arbitrary input (CONTl:SIGN:KDMI:MAIN:INP:LEV? to query the level on the assigned port)

Input

3  (Factory default), 4 (Factory default), 6 (Factory default)

LOW

Set the Low (Output Low level) at the assigned port.

Output

1, 2, 3 or 4

HIGH

Set the High (Output High level) at the assigned port

Output

1 (Factory default), 2 (Factory default) , 3 or 4

CHANNEL_CTRL

Function is controlled per channel. Define the function by :CONTrol:SIGNal:KDMI:MAIN:CHANnel:FUNCtion

N/A

1, 2, 3 or 4

NF_SOURCEx (x=1,2,...) *1

Noise Figure source switch control for port x

Ouptpu

1, 2, 3 or 4

NF_RECEIVERx (x=1,2,...) *1

Noise Figure receiver switch control for port x

Output

1, 2, 3 or 4

NF_LOy (y=1,2,…)

Noise Figure LO switch control for module y

Output

1, 2, 3 or 4

*1) For Noise Figure switch control, the signal is asserted no matter which ports are used in the NF channel if the port/module index(x) is not specified.

Examples

CONT:SIGN:KDMI:MAIN1:FUNC "LOW"

control:signal:kdmi:main2:function "NF_LO1"

Query Syntax

CONTrol:SIGNal:KDMI:MAIN:FUNC?

Return Type

<sting>

Default

See the table in <func>


CONTrol:SIGNal:KDMI:MAIN<port>:FUNCtion:CATalog?

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Read Only) Read the list of the available function for the specified port in the main control of the I/O adapter interface.  Example, "RF_PULSE_MOD_IN, INPUT1" is returned for the port 5.

For more information, see I/O Connector Interface

Parameters

 

<port>

Port Number. The number of total ports is returned by CONTrol:SIGNal:KDMI:MAIN:COUNt?.

Examples

CONT:SIGN:KDMI:MAIN:FUNC:CAT?

control:signal:kdmi:main:function:catalog?

Query Syntax

CONTrol:SIGNal:KDMI:MAIN:FUNC:CAT?

Return Type

<sting>, available function list with Comma separated chars

Default

See the table in <func> of  CONTrol:SIGNal:KDMI:MAIN:FUNC?


CONTrol:SIGNal:KDMI:MAIN<port>:INPut:LEVel?

Applicable Models: M980xA, M983xA, P50xxA/B, P93xxB

(Read only) Read the level of the specified INPUT port of the I/O adapter main side. This command reads the level immediately after its execution. It is not necessary to assign the port as INPUT by CONTrol:SIGNal:KDMI:MAIN:FUNCion command.  When the specified port is not input port, "Specified KDMI port is not input port" error is returned.

For more information, see I/O Connector Interface

Parameters

 

<port>

Port Number (3 to 6)

Examples

CONT:SIGN:KDMI:MAIN3:INP:LEV?

control:signal:kdmi:main3:input:level?

Query Syntax

CONTrol:SIGNal:KDMI:MAIN:INPut:LEVel?

Return Type

Char ("HIGH" or "LOW")

Default

N/A


CONTrol:SIGNal:KDMI:SUB:COUNt?

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Read only) Read the number of ports in the sub control of the I/O adapter interface.  In case for the M980xA/P50xxA, always 6.

For more information, see I/O Connector Interface

Parameters

None

Examples

CONT:SIGN:KDMI:SUB:COUN?

control:signal:kdmi:sub:count?

Query Syntax

CONTrol:SIGNal:KDMI:SUB:COUNt?

Return Type

Numeric value

Default

6


CONTrol:SIGNal:KDMI:SUB<port>:CHANnel<ch>:FUNCtion <func>

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Write-Read) Set and Read the function for the specified port and specified channel in the sub control port of the I/O adapter interface.  To use this, set CONTrol:SIGNal:KDMI:SUB:FUNCion at CHANNEL_CTRL. The setting is saved in th state file and subject to preset. Function can be selected from Output signal.

Parameters

 

<port>

Port Number. The number of total ports is returned by CONTrol:SIGNal:KDMI:SUB:COUNt?.

<ch>

Channel Number.

<func>

function name

Function name

Description

Type

Assignable pot number

READY_FOR_TRIGGER

Ready for trigger

Output

3

TRIGGER_OUT

AUX trigger

Output

4

INDEX

index

Output

5

SWEEP_END

Sweep end

Output

6

LOW

Set the Low at the assigned port

Output

3, 4, 5 or 6

HIGH

Set the High at the assigned port

Output

3, 4, 5 or 6

NF_RECEIVERx (x=1,2,...) *1

Noise Figure receiver switch control for port x

Output

3, 4, 5 or 6

NF_LOy (y=1,2,…)

Noise Figure LO switch control for module y

Output

3, 4, 5 or 6

*1) For Noise Figure switch control, the signal is asserted no matter which ports are used in the NF channel if the port/module index(x) is not specified.

Examples

CONT:SIGN:KDMI:SUB3:FUNC "CHANNEL_CTRL"

CONT:SIGN:KDMI:SUB3:CHAN3:FUNC "LOW"

 

CONTrol:SIGNal:KDMI:SUB2:FUNCion "CHANNEL_CTRL"

control:signal:kdmi:sub2:chan2:function "INPUT4"

Query Syntax

CONTrol:SIGNal:KDMI:SUB:FUNCion?

Return Type

<sting>

Default

HIGH

 


CONTrol:SIGNal:KDMI:SUB<port>:FUNCtion <func>

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Write-Read) Set and Read the function for the specified port in the sub control port of the I/O adapter interface.  The assigned settings are preserved for each system configuration even after preset, firmware restart and power on/off.  The CONTrol:SIGNal:KDMI:SUB:CHANnel:FUNCion allows you to set the function independently for each channel.

For more information, see I/O Connector Interface

Parameters

 

<port>

Port Number. The number of total ports is returned by CONTrol:SIGNal:KDMI:SUB:COUNt?.

<func>

function name

Function name

Description

Type

Assignable pot number

TRIGGER_IN

External trigger

Input

1 (Factory default)

PULSE_SYNC_IN

Pulse synchronization

Input

2 (Factory default)

AUX_TRIG_IN

AUX trigger input

Input

2

READY_FOR_TRIGGER

Ready for trigger

Output

3

TRIGGER_OUT

AUX trigger

Output

4

INDEX

index

Output

5

SWEEP_END

Sweep end

Output

6

INPUT

Arbitrary input (CONTl:SIGN:KDMI:SUB:INP:LEV? to query the level on the assigned port)

Input

3  (Factory default), 4  (Factory default)

LOW

Set the Low at the assigned port

Output

3, 4, 5 or 6

HIGH

Set the High at the assigned port

Output

3, 4, 5  (Factory default) or 6  (Factory default)

CHANNEL_CTRL

Function is controlled per channel. Define the function by :CONTrol:SIGNal:KDMI:SUB:CHANnel:FUNCtion

N/A

3, 4, 5 or 6

NF_RECEIVERx (x=1,2,...) *1

Noise Figure receiver switch control for port x

Output

3, 4, 5 or 6

NF_LOy (y=1,2,…)

Noise Figure LO switch control for module y

Output

3, 4, 5 or 6

*1) For Noise Figure switch control, the signal is asserted no matter which ports are used in the NF channel if the port/module index(x) is not specified.

Examples

CONT:SIGN:KDMI:SUB3:FUNC "LOW"

control:signal:kdmi:sub2:function "INPUT4"

Query Syntax

CONTrol:SIGNal:KDMI:SUB:FUNCion?

Return Type

<sting>

Default

See the table in <func>


CONTrol:SIGNal:KDMI:SUB<port>:FUNCtion:CATalog?

Applicable Models: M980xA, M983xA,P50xxA/B, P93xxB

(Read Only) Read the list of the available function for the specified port in the sub control port of the I/O adapter interface.  Example, "TRIGGER_IN, INPUT3" is returned for the port 1.

For more information, see I/O Connector Interface

Parameters

 

<port>

Port Number. The number of total ports is returned by CONTrol:SIGNal:KDMI:SUB:COUNt?.

Examples

CONT:SIGN:KDMI:SUB:FUNC:CAT?

control:signal:kdmi:sub:function:catalog?

Query Syntax

CONTrol:SIGNal:KDMI:SUB:FUNC:CAT?

Return Type

<sting>, available function list with Comma separated chars

Default

See the table in <func> of  CONTrol:SIGNal:KDMI:SUB:FUNC?


CONTrol:SIGNal:KDMI:SUB<port>:INPut:LEVel?

Applicable Models: M980xA, M983xA, P50xxA/B, P93xxB

(Read only) Read the level of the specified INPUT port of the I/O adapter sub side. This command reads the level immediately after its execution. It is not necessary to assign the port as INPUT by CONTrol:SIGNal:KDMI:SUB:FUNCtion command. The When the specified port is not input port, "Specified KDMI port is not input port" error is returned.

For more information, see I/O Connector Interface

Parameters

 

<num>

Port Number (1 to 4)

Examples

CONT:SIGN:KDMI:SUB3:INP:LEV?

control:signal:kdmi:sub3:input:level?

Query Syntax

CONTrol:SIGNal:KDMI:MAIN:INPut:LEVel?

Return Type

Char ("HIGH" or "LOW")

Default

N/A


CONTrol:SIGNal:PXI:RTRigger[:STATe] <bool>

Applicable Models: M980xA, M983xA

(Write-Read) Turns ON / OFF Ready for Trigger output from Backplane Trigger Lines.

Parameters

 

<bool>

Choose from:

  • ON (or 1) - VNA DOES output ready for trigger signal from Backplane Trigger line

  • OFF (or 0) – VNA does NOT output ready for trigger signal from Backplane Trigger line.

Examples

CONT:SIGN:PXI:RTR 1

control:signal:pxi:rtrigger:stat off

Query Syntax

CONTrol:SIGNal:PXI:RTRigger[:STATe]?

Return Type

Boolean

Default

0 (Preset will not reset the setting.)


CONTrol:SIGNal:PXI:RTRigger:ROUTe <char>

Applicable Models: M980xA, M983xA

(Write-Read) Specifies the Backplane Trigger Line to use for the trigger OUT ready line.

Parameters

 

<char>

Choose from:

TRIG0 – Backplane Trigger Lines (PXI TRIG0)

TRIG1 – Backplane Trigger Lines (PXI TRIG1)

TRIG2 – Backplane Trigger Lines (PXI TRIG2)

TRIG3 – Backplane Trigger Lines (PXI TRIG3)

TRIG4 – Backplane Trigger Lines (PXI TRIG4)

TRIG5 – Backplane Trigger Lines (PXI TRIG5)

TRIG6 – Backplane Trigger Lines (PXI TRIG6)

TRIG7 – Backplane Trigger Lines (PXI TRIG7)

Examples

CONT:SIGN:PXI:RTR:ROUT TRIG0

control:signal:pxi:rtrigger:route trig0

Query Syntax

CONTrol:SIGNal:PXI:RTRigger:ROUTe?

Return Type

Character

Default

TRIG1


CONTrol:SIGNal:PXI:TRIGger:OUTPut[:STATe] <bool>

Applicable Models: M980xA, M983xA

(Write-Read) Turns ON / OFF the trigger output from PXI Backplane line when “CONTrol:SIGNal:TRIGger:OUTP[:STATe]” is “ON”.

Parameters

 

<bool>

ON (or 1) - VNA DOES output trigger signals from PXI Backplane when “CONTrol:SIGNal:TRIGger:OUTP[:STATe]” is “ON”.

OFF (or 0) – VNA does NOT output trigger signals from PXI Backplane.

Examples

CONT:SIGN:PXI:TRIG:OUTP 1

control:signal:pxi:trigger:output:stat off

Query Syntax

CONTrol:SIGNal:PXI:TRIGger:OUTPut[:STATe]?

Return Type

Boolean

Default

OFF


CONTrol:SIGNal:PXI:TRIGger:OUTPut:ROUTe <char>

Applicable Models: M980xA, M983xA

(Write-Read) Specifies the Backplane Trigger Line to use for the trigger output line.

Parameters

 

<char>

Choose from:

TRIG0 – Backplane Trigger Lines (PXI TRIG0)

TRIG1 – Backplane Trigger Lines (PXI TRIG1)

TRIG2 – Backplane Trigger Lines (PXI TRIG2)

TRIG3 – Backplane Trigger Lines (PXI TRIG3)

TRIG4 – Backplane Trigger Lines (PXI TRIG4)

TRIG5 – Backplane Trigger Lines (PXI TRIG5)

TRIG6 – Backplane Trigger Lines (PXI TRIG6)

TRIG7 – Backplane Trigger Lines (PXI TRIG7)

Examples

CONT:SIGN:PXI:TRIG:OUTP:ROUT TRIG0

control:signal:pxi:trigger:output:route trig0

Query Syntax

CONTrol:SIGNal:PXI:TRIGger:OUTPut:ROUTe?

Return Type

Character

Default

TRIG2


CONTrol:SIGNal:STReamline:RTRigger[:STATe] <bool>

Applicable Models: P50xxA/B, P93xxB

(Write-Read) Turns ON / OFF Ready for Trigger output from Streamline Rear SMB.

Parameters

 

<bool>

Choose from:

  • ON (or 1) - VNA DOES output ready for trigger signal from Streamline Rear SMB
  • OFF (or 0) – VNA does NOT output ready for trigger signal from Streamline Rear SMB

Examples

CONT:SIGN:STR:RTR 1

control:signal:streamline:rtrigger:stat off

Query Syntax

CONTrol:SIGNal:STReamline:RTRigger[:STATe]?

Return Type

Boolean

Default

0 (Preset will not reset the setting.)


CONTrol:SIGNal:STReamline:RTRigger:ROUTe <char>

Applicable Models: P50xxA/B, P93xxB

(Write-Read) Specifies the Backplane Trigger Line to use for the trigger OUT ready line.

Parameters

 

<char>

Choose from:

NONE – Streamline Rear SMB Not connected (NONE)

REAR1 – Streamline Rear SMB (TRIG1)

REAR2 – Streamline Rear SMB (TRIG2)

Examples

CONT:SIGN:STR:RTR:ROUT TRIG1

control:signal:streamline:rtrigger:route trig1

Query Syntax

CONTrol:SIGNal:STReamline:RTRigger:ROUTe?

Return Type

Character

Default

N/A


CONTrol:SIGNal:STReamline:TRIGger:OUTPut[:STATe] <bool>

Applicable Models: P50xxA/B, P93xxB

(Write-Read) Turns ON / OFF the trigger output from Streamline Rear SMB when “CONTrol:SIGNal:TRIGger:OUTP[:STATe]” is “ON”.

Parameters

 

<bool>

ON (or 1) - VNA DOES output trigger signals from Streamline Rear SMB when  “CONTrol:SIGNal:TRIGger:OUTP[:STATe]” is “ON”.

OFF (or 0) – VNA does NOT output trigger signals from Streamline Rear SMB.

Examples

CONT:SIGN:STR:TRIG:OUTP 1

control:signal:streamline:trigger:output:stat off

Query Syntax

CONTrol:SIGNal:STReamline:TRIGger:OUTPut[:STATe]?

Return Type

Boolean

Default

OFF


CONTrol:SIGNal:STReamline:TRIGger:OUTPut:ROUTe <char>

Applicable Models: P50xxA/B, P93xxB

(Write-Read) Specifies the Streamline Rear SMB to use for the trigger output line.

Parameters

 

<char>

Choose from:

NONE – Streamline Rear SMB Not connected (NONE)

REAR1 – Streamline Rear SMB (REAR TRIG1)

REAR2 – Streamline Rear SMB (REAR TRIG2)

Examples

CONT:SIGN:STR:TRIG:OUTP:ROUT REAR1

control:signal:streamline:trigger:output:route rear1

Query Syntax

CONTrol:SIGNal:STReamline:TRIGger:OUTPut:ROUTe?

Return Type

Character

Default

REAR2