:CHANnel:PROBe:ACCessories:ATTenuator:SELect
Command Syntax
:CHANnelN:PROBe:ACCessories:ATTenuator:SELect "<model>"
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
The command parameter is a quoted model number string. The available model number strings are shown in the Infiniium graphical user interface (GUI) or in the GUI's Interactive SCPI Command Tree.
Query Syntax
:CHANnelN:PROBe:ACCessories:ATTenuator:SELect?
Description
Selects a known Keysight probe attenuator (with known compensation values).
To turn on and off compensation for the selected Keysight probe attenuator, use the :CHANnel:PROBe:ACCessories:ATTenuator:STATe command.
When using a probe attenuator that is not a known Keysight model, it can be considered external hardware, and you can specify its attenuation/gain/dB settings using the :CHANnel External Scaling Commands.