:CHANnel:PROBe:ACCessories:ECABle:STATe
Command Syntax
:CHANnelN:PROBe:ACCessories:ECABle:STATe {OFF | ON}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:PROBe:ACCessories:ECABle:STATe?
Description
Turns on and off compensation for the selected Keysight extension cable.
You can select from a list of Keysight extension cables using the :CHANnel:PROBe:ACCessories:ECABle:SELect command, and the proper attenuation settings will be known.
When using an extension cable that is not a known Keysight model, it can be considered external hardware, and you can specify its attenuation/gain/dB settings using the :CHANnel External Scaling Commands.