:DISK:PROTocol:FNAMe:USTandard
Command Syntax
:DISK:PROTocol:FNAMe:USTandard
Description
Resets the file name for the protocol decode file from using a custom name to using the standard name in the following form:
Protocol_Symbol_File_<date><autonumber>.<extension>
For example, Protocol_Symbol_File_2020-10-23_1.csv. Refer to :DISK:PROTocol:FNAMe to learn about standard and custom names.