:DISK:PROTocol:SAVE:SOURce
Command Syntax
:DISK:PROTocol:SAVE:SOURce <protocol_decode>
Where <protocol_decode> can be one of the following:
PROTocol{1:4}
Query Syntax
:DISK:PROTocol:SAVE:SOURce?
Description
Selects the protocol decode for saving to a file.
Use the :DISK:PROTocol:SAVE:LISTing command to select the symbol listing or packet listing within the selected protocol decode to save.
Use :DISK:PROTocol:SAVE to actually save the file.