:DISK:PROTocol:SAVE:LISTing

Command Syntax

:DISK:PROTocol:SAVE:LISTing <listing>

Where <listing> can be one of the following:

  • SLISting{1:4} — Symbol listing.
  • PLISting{1:4} — Packet listing.

Query Syntax

:DISK:PROTocol:SAVE:LISTing?

Description

Selects the symbol listing or packet listing from within the selected protocol decode (see :DISK:PROTocol:SAVE:SOURce) for saving to a file. Use :DISK:PROTocol:SAVE to actually save the file.

Parent Command