:FUNCtion:FOPerator:STATus?

Query Syntax

:FUNCtionN:FOPerator:STATus?

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Description

Queries the status of a function's definition. Some functions require configuration after being created using the :FUNCtion:FOPerator parent command.

CORR
The function definition is correct and complete.
INV
The function needs configuration to be complete. Use the :FUNCtion:FOPerator:STATus:REASon? child command to return a string that indicates the missing information.

Child Commands

Parent Command