:FUNCtion:FOPerator:STATus:REASon?

Query Syntax

:FUNCtionN:FOPerator:STATus:REASon?

Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.

Description

Returns a string that indicates the information required to correctly configure a function. For example, the string "Please select a file" would be returned for an incomplete Apply s2p operator.

Parent Command