:FUNCtion:FOPerator:STATus:DETails?
Query Syntax
:FUNCtionN:FOPerator:STATus:DETails?
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Description
If the status of the function definition is questionable or invalid (see :FUNCtion:FOPerator:STATus?), this query returns a string that may provide additional details.
If the status of the function definition is valid, this query returns an empty string.
For a basic reason for the questionable or invalid status, use the :FUNCtion:FOPerator:STATus:REASon? sibling query.
For user-defined function operators (USER, BUSer, TUSer, or QUSer), only the first error from the script is returned by this query.