:GRAPh:DBHertz:X:STARt
Command Syntax
:GRAPh:DBHertzN:X:STARt <frequency>
<frequency> is a double.
Where N specifies one of four {1:4} waveform content windows.
Query Syntax
:GRAPh:DBHertzN:X:STARt?
Description
For the specified Freq-Magwaveform content window, sets the graph's X- axis start frequency in Hertz. Use the :GRAPh:DBHertz:X:AUToscale sibling command to automatically set the center, span, start, and stop settings. Use the :GRAPh:DBHertz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.