:GRAPh:DBHertz:Y:OFFSet
Command Syntax
:GRAPh:DBHertzN:Y:OFFSet <dB>
<dB> is a double.
Where N specifies one of four {1:4} waveform content windows.
Query Syntax
:GRAPh:DBHertzN:Y:OFFSet?
Description
Sets the vertical offset of the specified Decibels (Hz) content window with respect to the Y-axis's reference level (:GRAPh:DBHertz:Y:REFerence).
Use the :GRAPh:DBHertz:Y:AUToscale sibling command to automatically set the offset and scale settings.
Use the :GRAPh:DBHertz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.