:GRAPh:DBHertz:Y:SCALe

Command Syntax

:GRAPh:DBHertzN:Y:SCALe <scale>

<scale> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:DBHertzN:Y:SCALe?

Description

Sets the vertical scale of the specified Decibels (Hz) content window in dB-per-division. The vertical expansion and contraction is referenced to the center graticule (:GRAPh:DBHertz:Y:OFFSet sibling command) of the display. Use the :GRAPh:DBHertz:Y:AUToscale sibling command to automatically set the offset and scale settings. Use the :GRAPh:DBHertz:AUToscale parent command to automatically scale both the waveform in both X and Y axis.