:GRAPh:IRESponse:X:SPAN
Command Syntax
:GRAPh:IRESponseN:X:SPAN <frequency>
<frequency> is a double.
Where N specifies one of four {1:4} waveform content windows.
Query Syntax
:GRAPh:IRESponseN:X:SPAN?
Description
For the specified Impulse Response waveform content window, sets the graph's X- axis time span in seconds. Use the :GRAPh:IRESponse:X:AUToscale sibling command to automatically set the center, span, start, and stop settings. Use the :GRAPh:IRESponse:AUToscale parent command to automatically scale both the waveform in both X and Y axis.