:GRAPh:IRESponse:Y:OFFSet
Command Syntax
:GRAPh:IRESponseN:Y:OFFSet <degrees>
<degrees> is a double.
Where N specifies one of four {1:4} waveform content windows.
Query Syntax
:GRAPh:IRESponseN:Y:OFFSet?
Description
Sets the vertical offset of the specified Impulse Response content window at the Y-axis's center graticule. Use the :GRAPh:IRESponse:Y:AUToscale sibling command to automatically set the offset and scale settings. Use the :GRAPh:IRESponse:AUToscale parent command to automatically scale both the waveform in both X and Y axis.