:GRAPh:IRESponse:X:STOP

Command Syntax

:GRAPh:IRESponseN:X:STOP <frequency>

<frequency> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:IRESponseN:X:STOP?

Description

For the specified Impulse Response waveform content window, sets the graph's X- axis stop time in seconds. Use the :GRAPh:IRESponse:X:AUToscale sibling command to automatically set the center, span, start, and stop settings. Use the :GRAPh:IRESponse:AUToscale parent command to automatically scale both the waveform in both X and Y axis.