:GRAPh:SRESponse:Y:OFFSet

Command Syntax

:GRAPh:SRESponseN:Y:OFFSet <degrees>

<degrees> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:SRESponseN:Y:OFFSet?

Description

Sets the vertical offset of the specified Step Response content window at the Y-axis's center graticule. Use the :GRAPh:SRESponse:Y:AUToscale sibling command to automatically set the offset and scale settings. Use the :GRAPh:SRESponse:AUToscale parent command to automatically scale both the waveform in both X and Y axis.