:GRAPh:SRESponse:Y:REFerence
Command Syntax
:GRAPh:SRESponseN:Y:REFerence {CENTer}
Where N specifies one of four {1:4} waveform content windows.
Query Syntax
:GRAPh:SRESponseN:Y:REFerence?
Description
Sets the vertical reference location of the specified Step Response content window to be located at the graticule's vertical center.
The :GRAPh:SRESponse:Y:OFFSet is the value at the vertical reference location.
You can adjust the :GRAPh:SRESponse:Y:OFFSet value to, in essence, move the zero level about the reference location. When the :GRAPh:SRESponse:Y:OFFSet value is zero, the zero level is at the vertical reference location.