:GRAPh:SRESponse:Y:SCALe

Command Syntax

:GRAPh:SRESponseN:Y:SCALe <scale>

<scale> is a double.

Where N specifies one of four {1:4} waveform content windows.

Query Syntax

:GRAPh:SRESponseN:Y:SCALe?

Description

Sets the vertical scale of the specified Step Response content window. The vertical expansion and contraction is referenced to the center graticule (:GRAPh:SRESponse:Y:OFFSet sibling command) of the display. Use the :GRAPh:SRESponse:Y:AUToscale sibling command to automatically set the offset and scale settings. Use the :GRAPh:SRESponse:AUToscale parent command to automatically scale both the waveform in both X and Y axis.