:LTESt:ACQuire:SIMage:INVert
Command Syntax
:LTESt:ACQuire:SIMage:INVert {ON | OFF | 1 | 0}
Query Syntax
:LTESt:ACQuire:SIMage:INVert?
Query Response
{1 | 0}
Description
Turns on and off the inversion of the graticule area's background color when reporting a screen capture for an acquisition limit test.
When on, an inverted image will be captured and saved into a file by the :LTESt:ACQuire:SIMage:FNAMe command. The entire application window is saved with the graticule black upon a white background. The waveform colors remain unchanged. Use the :LTESt:ACQuire:SIMage:STATe command to enable and disable screen-capture reporting. To enable or disable acquisition limit tests, use the :LTESt:ACQuire:STATe command.