:LTESt:ACQuire:SIMage:WINDow
Command Syntax
:LTESt:ACQuire:SIMage:WINDow {DISPlay | TIME{1} | SHERtz{1:4} | DBHertz{1:4} | DHERtz{1:4}}
Query Syntax
:LTESt:ACQuire:SIMage:WINDow?
Query Response
{1 | 0}
Description
When reporting a screen image as a result of an acquisition limit test, use this command to selects which portion of the screen to include in the image. To actually specify that a screen image is saved, use the :LTESt:ACQuire:SIMage:STATe command. The following selections are available:
- DISPlay
- Includes the entire Infiniium 2026 screen in the captured screen image.
- TIMe1
- Includes only the Waveform content window in the captured screen image.
- SHERtz{1:4}
- Includes only the Delay 1, Delay 2, Delay 3, or Delay 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Delay windows 2, 3, and 4 can only be displayed programmatically and not using front-panel controls. The group Delay window can be selected as a display output format for FFT functions (
:FUNCtion:FOPerator FFT). - DBHertz{1:4}
- Includes only the Decibels (Hz) 1, Decibels (Hz) 2, Decibels (Hz) 3, or Decibels (Hz) 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Decibels (Hz) windows 2, 3, and 4 can only be displayed programmatically and not using front-panel controls. The group Decibels (Hz) window can be selected as a display output format for FFT functions (
:FUNCtion:FOPerator FFT). - DHERtz{1:4}
- Includes only the Degrees (Hz) 1, Degrees (Hz) 2, Degrees (Hz) 3, or Degrees (Hz) 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Degrees (Hz) windows 2, 3, and 4 can only be displayed programmatically and not using front-panel controls. The group Degrees (Hz) window can be selected as a display output format for FFT functions (
:FUNCtion:FOPerator FFT).