:LTESt:ACQuire:SIMage:STATe
Command Syntax
:LTESt:ACQuire:SIMage:STATe {ON | OFF | 1 | 0}
Query Syntax
:LTESt:ACQuire:SIMage:STATe?
Query Response
{1 | 0}
Description
Selects to save a screen image to a file after the limit test acquires the specified number of waveforms, samples, or patterns. Use the :LTESt:ACQuire:CTYPe command and its :WAVeforms, :SAMPles, or :PATTerns child commands to specify the test conditions required to end the test. Use the commands shown in the following table to configure the output file.
| Task | Command |
|---|---|
| Enter the filename and path | :LTESt:ACQuire:SIMage:FNAMe
|
| Enter the graphics file type | :LTESt:ACQuire:SIMage:FTYPe?
|
| Select portion of Infiniium display to capture | :LTESt:ACQuire:SIMage:WINDow
|
| Include metadata in jpg and tiff files. | :LTESt:ACQuire:SIMage:IMETadata
|
| Invert background color | :LTESt:ACQuire:SIMage:INVert
|
| Black and white output | :LTESt:ACQuire:SIMage:MONochrome
|
| Capture a single waveform among several displayed waveforms | :LTESt:ACQuire:SIMage:SINClude
|