:MEASure:CLOCk:CTIerror
Command Syntax
:MEASure:CLOCk:CTIerror
Query Syntax
:MEASure:CLOCk:CTIerror?
Description
This command moves the Clock TIE (Time Interval Error) measurement to the top of the Results table and displays the measurement if it is not already shown on the table.
The query form of the command returns the measured value.
To measure Clock TIE (Time Interval Error), :CRECovery:MODE must be performed to determine the clock locations.
Once the ideal clock frequency is determined, all of the cycles of your waveform are compared to the ideal clock frequency and the error statistics are computed. The following figure shows how the Clock TIE is measured on rising edges of the clock.
Use :MEASure:CLOCk:CTIerror:REGion to specify the waveform data region over which the measurement is made.
Sources can be any displayed waveform, waveform memory, or function. For example, CHAN1_1, WMEMory1, or FUNCtion1.
Use :MEASure:TBASe:GENeral:METHod to change the definition of the waveform's top/base. Use :<waveform>:THReshold:GENeral:METHod to change the definition of the waveform's threshold.
If you want to apply a filter to the TIE measurement, see :MEASure:CLOCk:CTIerror:TIEFilter.
Example Command Sequence
:MEASure:CLOCk:CTIerror:SOURce CHAN1_1 :MEASure:CLOCk:CTIerror:EDIRection RISing :MEASure:CLOCk:CTIerror :MEASure:CLOCk:CTIerror?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Infiniium.query(':MEASure:CLOCk:CTIerror:STATus?')):
measurement = Infiniium.query(':MEASure:CLOCk:CTIerror?')
If averaging is turned on (:ACQuire:SMODe AVERage), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:COUNt?) versus the number of measurement sweeps that have occurred (:ACQuire:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Infiniium.query(':MEASure:CLOCk:CTIerror:COUNt?') >= Infiniium.query(':ACQuire:COUNt?')):
measurement = Infiniium.query(':MEASure:CLOCk:CTIerror?')
You can also use an acquisition limit test to test that a number of waveforms or samples have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Querying Measurement Results and Statistics
You can query measurement results using the :MEASure:CLOCk:CTIerror? query after making the proper instance settings.
If a measurement is installed into Results table (using the :MEASure:CLOCk:CTIerror command) and you have made the proper instance settings, you can query statistics using common child queries.
Also, you can query measurement results and statistics directly from the Results table (without having to make the proper instance settings beforehand). See Querying Measurement Results and Statistics.