:MEASure:CLOCk:CTIerror:EDIRection
Command Syntax
:MEASure:CLOCk:CTIerror:EDIRection {RISing | FALLing | BOTH}
Query Syntax
:MEASure:CLOCk:CTIerror:EDIRection?
Description
For the Clock TIE measurement (see :MEASure:CLOCk:CTIerror), specifies the waveform's edges to be measured: rising, falling or both edges.
When BOTH is selected, there will be annotations for both the rising edge measurement and the falling edge measurement.
Example Command Sequence
This sequence sets up the measurement on rising edges only.
:MEASure:CLOCk:CTIerror:SOURce CHAN1_1
:MEASure:CLOCk:CTIerror:EDIRection RISing
// Perform measurement
:MEASure:CLOCk:CTIerror
:MEASure:CLOCk:CTIerror?