Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MEASure:CLOCk:CTIerror:STATus:DETails?

Clock TIE Commands
  • :MEASure:CLOCk:CTIerror
  • :MEASure:CLOCk:CTIerror:EDIRection
  • :MEASure:CLOCk:CTIerror:FAVorite
  • :MEASure:CLOCk:CTIerror:LOCation?
  • :MEASure:CLOCk:CTIerror:OCCurrences
  • :MEASure:CLOCk:CTIerror:REGion
  • :MEASure:CLOCk:CTIerror:SOURce
  • :MEASure:CLOCk:CTIerror:STATus?
  • :MEASure:CLOCk:CTIerror:STATus:DETails?
  • :MEASure:CLOCk:CTIerror:STATus:REASon?
  • :MEASure:CLOCk:CTIerror:TIEFilter
  • :MEASure:CLOCk:CTIerror:TIEFilter:DFACtor
  • :MEASure:CLOCk:CTIerror:TIEFilter:SHAPe
  • :MEASure:CLOCk:CTIerror:TIEFilter:STARt
  • :MEASure:CLOCk:CTIerror:TIEFilter:STOP
  • :MEASure:CLOCk:CTIerror:TIEFilter:TYPE
  • :MEASure:CLOCk:CTIerror:UNITs
  • :MEASure:CLOCk:CTIerror:UREFerence:STATe
  • :MEASure:CLOCk:CTIerror:UREFerence:VALue

Query Syntax

:MEASure:CLOCk:CTIerror:STATus:DETails?

Description

Returns a string that may provide additional details for a failed :MEASure:CLOCk:CTIerror measurement. If the measurement was successful, a null string is returned.

For a basic description of a measurement failure, use the :MEASure:CLOCk:CTIerror:STATus:REASon? sibling query. Use the :STATus? parent query to determine if the measurement has failed.

See Also

  • Measurement Errors