:MEASure:DATA:DTIerror

Command Syntax

:MEASure:DATA:DTIerror

Query Syntax

:MEASure:DATA:DTIerror?

Description

This command moves the Data TIE (Time Interval Error) measurement to the top of the Results table and displays the measurement if it is not already shown on the table.

The query form of the command returns the measured value.

To measure Data TIE (Time Interval Error), :CRECovery:MODE must be performed to determine the clock locations.

Once the clock locations are determined, midpoints between clock locations are compared to edge crossings at the measurement threshold. Differences from the measured edge location and ideal edge location are computed. The following figure shows how the Data TIE is measured.

Use :MEASure:DATA:DTIerror:REGion to specify the waveform data region over which the measurement is made.

Sources can be any displayed waveform, waveform memory, or function. For example, CHAN1_1, WMEMory1, or FUNCtion1.

Use :MEASure:TBASe:GENeral:METHod to change the definition of the waveform's top/base. Use :<waveform>:THReshold:GENeral:METHod to change the definition of the waveform's threshold.

If you want to apply a filter to the TIE measurement, see :MEASure:DATA:DTIerror:TIEFilter.

Example Command Sequence

:MEASure:DATA:DTIerror:SOURce CHAN1_1
:MEASure:DATA:DTIerror
:MEASure:DATA:DTIerror?

Measurement Ready?

To confirm that the measurement is ready to read, you can query the measurement's status:

if ('CORR' in Infiniium.query(':MEASure:DATA:DTIerror:STATus?')):
	measurement = Infiniium.query(':MEASure:DATA:DTIerror?')

If averaging is turned on (:ACQuire:SMODe AVERage), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:COUNt?) versus the number of measurement sweeps that have occurred (:ACQuire:COUNt?). The technique uses the :COUNt? common measurement query. For example,

if (Infiniium.query(':MEASure:DATA:DTIerror:COUNt?') >= Infiniium.query(':ACQuire:COUNt?')):
	measurement = Infiniium.query(':MEASure:DATA:DTIerror?')

You can also use an acquisition limit test to test that a number of waveforms or samples have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.

Querying Measurement Results and Statistics

You can query measurement results using the :MEASure:DATA:DTIerror? query after making the proper instance settings.

If a measurement is installed into Results table (using the :MEASure:DATA:DTIerror command) and you have made the proper instance settings, you can query statistics using common child queries.

Also, you can query measurement results and statistics directly from the Results table (without having to make the proper instance settings beforehand). See Querying Measurement Results and Statistics.