Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MEASure:DATA:DTIerror:STATus:REASon?

Data TIE Commands
  • :MEASure:DATA:DTIerror
  • :MEASure:DATA:DTIerror:EYE
  • :MEASure:DATA:DTIerror:FAVorite
  • :MEASure:DATA:DTIerror:LOCation?
  • :MEASure:DATA:DTIerror:OCCurrences
  • :MEASure:DATA:DTIerror:REGion
  • :MEASure:DATA:DTIerror:SOURce
  • :MEASure:DATA:DTIerror:STATus?
  • :MEASure:DATA:DTIerror:STATus:DETails?
  • :MEASure:DATA:DTIerror:STATus:REASon?
  • :MEASure:DATA:DTIerror:TIEFilter
  • :MEASure:DATA:DTIerror:TIEFilter:DFACtor
  • :MEASure:DATA:DTIerror:TIEFilter:SHAPe
  • :MEASure:DATA:DTIerror:TIEFilter:STARt
  • :MEASure:DATA:DTIerror:TIEFilter:STOP
  • :MEASure:DATA:DTIerror:TIEFilter:TYPE
  • :MEASure:DATA:DTIerror:UNITs
  • :MEASure:DATA:DTIerror:UREFerence:STATe
  • :MEASure:DATA:DTIerror:UREFerence:VALue

Query Syntax

:MEASure:DATA:DTIerror:STATus:REASon?

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :MEASure:DATA:DTIerror measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :MEASure:DATA:DTIerror:STATus:DETails? sibling query. Use the :MEASure:DATA:DTIerror:STATus? parent query to determine if the measurement has failed.

See Also

  • Measurement Errors