:MEASure:DATA:DTIerror:EYE
Command Syntax
:MEASure:DATA:DTIerror:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:DATA:DTIerror:EYE?
Description
If the selected signal is a PAM signal type (see the :<source>:SIGNal:TYPE command), this command specifies which eye threshold will be used to make the measurement.
For example, for PAM4 you can select EYE0 for the 0/1 eye threshold, EYE1 for the 1/2 eye threshold, or EYE2 for the 2/3 eye threshold.