:MEASure:EYE:JITTer:DEFine:SIGNal

Command Syntax

:MEASure:EYE:JITTer:DEFine:SIGNal {CLOCk | DATA}

Query Syntax

:MEASure:EYE:JITTer:DEFine:SIGNal?

Description

Specifies the type of input signal: data (DATA) or clock (CLOCk). Use this command if a poorly-defined signal cannot be automatically detected using :MEASure:EYE:JITTer:DEFine:SIGNal:AUTodetect.

Example Command Sequence

:MEASure:EYE:JITTer:DEFine:SIGNal:AUTodetect OFF
:MEASure:EYE:JITTer:DEFine:SIGNal CLOCk