:MEASure:EYE:JITTer:DEFine:UNITs

Command Syntax

:MEASure:EYE:JITTer:DEFine:UNITs {SECond | UINTerval}

Query Syntax

:MEASure:EYE:JITTer:DEFine:UNITs?

Description

Selects measurement units for Jitter values that are reported in the Results table and shown on the x-axis of displayed graphs. Choices are seconds (default value) or Unit Interval (UI), which is the symbol period of the data.