:MEASure:EYE:JITTer:DEFine:SIGNal:AUTodetect
Command Syntax
:MEASure:EYE:JITTer:DEFine:SIGNal:AUTodetect {{ON | 1} | {OFF | 0}}
Query Syntax
:MEASure:EYE:JITTer:DEFine:SIGNal:AUTodetect?
Query Response
{1 | 0}
Description
Selects to automatically detect the type of input signal: data or clock. The default is autodetection (ON). If a poorly-defined signal cannot be automatically detected, turn off automatic detection specify the signal type with the :MEASure:EYE:JITTer:DEFine:SIGNal command.