:MEASure:EYE:USER:USER{N}:COMMents?

Query Syntax

:MEASure:EYE:USER:USER{1:8}:COMMents?

Description

Returns the comment string for the selected user measurement. The comment string is defined in the measurement's XML definition file using the <Comments> tag. The comment string is limited in length to 512 characters.

Use the :MEASure:EYE:USER:USER{N} parent command to turn on the measurement and return the measured value.