Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MEASure:EYE:USER:USER{N}:STATus:REASon?

User-Defined Eye Measurement Commands
  • :MEASure:EYE:USER:USER{N}
  • :MEASure:EYE:USER:USER{N}:ABBReviation?
  • :MEASure:EYE:USER:USER{N}:CFILe
  • :MEASure:EYE:USER:USER{N}:CFILe:CLEar
  • :MEASure:EYE:USER:USER{N}:CFILe:RELoad
  • :MEASure:EYE:USER:USER{N}:CFLoaded?
  • :MEASure:EYE:USER:USER{N}:COMMents?
  • :MEASure:EYE:USER:USER{N}:FAVorite
  • :MEASure:EYE:USER:USER{N}:LOCation?
  • :MEASure:EYE:USER:USER{N}:LSTatus?
  • :MEASure:EYE:USER:USER{N}:LSTatus:DETails?
  • :MEASure:EYE:USER:USER{N}:LSTatus:REASon?
  • :MEASure:EYE:USER:USER{N}:NAME?
  • :MEASure:EYE:USER:USER{N}:SOURce{1:2}
  • :MEASure:EYE:USER:USER{N}:STATus?
  • :MEASure:EYE:USER:USER{N}:STATus:DETails?
  • :MEASure:EYE:USER:USER{N}:STATus:REASon?

Query Syntax

:MEASure:EYE:USER:USER{1:8}:STATus:REASon?

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :MEASure:EYE:USER:USER{N} measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :MEASure:EYE:USER:USER{N}:STATus:DETails? sibling query. Use the :MEASure:EYE:USER:USER{N}:STATus? parent query to determine if the measurement has failed.

See Also

  • Measurement Errors