:MEASure:EYE:USER:USER{N}:LSTatus:DETails?
Query Syntax
:MEASure:EYE:USER:USER{1:8}:LSTatus:DETails?
Description
If the status of the configuration file load is questionable or invalid (see :MEASure:EYE:USER:USER{N}:LSTatus?), this query returns a string that may provide additional details.
If the status of the configuration file load is valid, this query returns an empty string.
For a basic reason for the questionable or invalid status, use the :MEASure:EYE:USER:USER{N}:LSTatus:REASon? sibling query.