:MEASure:HORizontal:BWIDth:OCCurrences
Command Syntax
:MEASure:HORizontal:BWIDth:OCCurrences {ONE | ALL}
Query Syntax
:MEASure:HORizontal:BWIDth:OCCurrences?
Description
This command lets you select between Measure One and Measure All in the user interface which specifies whether Infiniium should make one edge-related measurement per acquisition or multiple measurements per acquisition using all edges in the acquisition.
When Measure One is selected:
- Measurements using edges are made on a particular edge (or pair of edges). Measurements are made on the edge closest to the timebase reference (see
:TIMebase:REFerence). - Measurement statistics are calculated for the one specific edge only and compiled over a number of acquisitions. A Single acquisition adds a single value to the measurement statistics. All other edges are ignored.
When Measure All is selected:
- Measurements using edges are made on all edges (or all pairs of edges) in the acquisition.
-
The "Current" measurement result (see
:MEASure:RESults?) is taken from the measurement closest to the timebase reference. For measurements on memory waveforms, it is the measurement closest to the horizontal X position setting. Annotations are shown at the "Current" measurement result.
Switching between Measure One and Measure All restarts the measurement count.
Query Response
{ONE | ALL}