:TIMebase:REFerence
Command Syntax
:TIMebase:REFerence {LEFT | DIVision1 | CENTer | RIGHt}
Query Syntax
:TIMebase:REFerence?
Description
Selects the horizontal reference position to be located at the graticule's left side, 1st division, center, or right side.
The :TIMebase:POSition value is the location of the reference with respect to the trigger (t=0).
You can adjust the :TIMebase:POSition value to, in essence, move the trigger position about the reference location. When the :TIMebase:POSition value is zero, the trigger position is the same as the horizontal reference location.