:MEASure:HORizontal:EEDGe:EDIRection{1:2}
Command Syntax
:MEASure:HORizontal:EEDGe:EDIRection{1:2} {RISing | FALLing | EITHer}
Query Syntax
:MEASure:HORizontal:EEDGe:EDIRection?
Description
For the Edge to Edge (:MEASure:HORizontal:EEDGe) measurement, this command specifies the waveform's edge direction used to identify the first or second measurement edge: rising, falling or either.
To set the edge threshold, use the :MEASure:HORizontal:EEDGe:ETHReshold{1:2} command.