:MEASure:HORizontal:EEDGe:ETHReshold{1:2}

Command Syntax

:MEASure:HORizontal:EEDGe:ETHReshold{1:2}  {UPPer | MIDDle | LOWer}

Query Syntax

:MEASure:HORizontal:EEDGe:ETHReshold?

Description

For the Edge to Edge (:MEASure:HORizontal:EEDGe) measurement, this command specifies the waveform's edge threshold to be used to identify the first or second edge in the measurement.

To set the edge direction, use the :MEASure:HORizontal:EEDGe:EDIRection{1:2} command.