Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MEASure:HORizontal:EEDGe:MODE

Edge to Edge Commands
  • :MEASure:HORizontal:EEDGe
  • :MEASure:HORizontal:EEDGe:EDIRection{1:2}
  • :MEASure:HORizontal:EEDGe:ETHReshold{1:2}
  • :MEASure:HORizontal:EEDGe:FAVorite
  • :MEASure:HORizontal:EEDGe:LOCation?
  • :MEASure:HORizontal:EEDGe:MODE
  • :MEASure:HORizontal:EEDGe:OCCurrences
  • :MEASure:HORizontal:EEDGe:REGion
  • :MEASure:HORizontal:EEDGe:SOURce
  • :MEASure:HORizontal:EEDGe:STATus?
  • :MEASure:HORizontal:EEDGe:STATus:DETails?
  • :MEASure:HORizontal:EEDGe:STATus:REASon?
  • :MEASure:HORizontal:EEDGe:STRide
  • :MEASure:HORizontal:EEDGe:UREFerence:STATe
  • :MEASure:HORizontal:EEDGe:UREFerence:VALue

Command Syntax

:MEASure:HORizontal:EEDGe:MODE {NEXT | PREVious}

Query Syntax

:MEASure:HORizontal:EEDGe:MODE?

Description

For the :MEASure:HORizontal:EEDGe measurement, this command specifies whether to measure the next or previous specified edge on the second source.