:MEASure:HORizontal:TVOLt:ENUMber
Command Syntax
:MEASure:HORizontal:TVOLt:ENUMber <edge_number>
Query Syntax
:MEASure:HORizontal:TVOLt:ENUMber?
Description
For the Time-at-Amplitude measurement, specifies the edge number used to identify the waveform location at which to perform the measurement. To specify the edge direction, use the :MEASure:HORizontal:TVOLt:EDIRection command. To specify the amplitude value, use the :MEASure:HORizontal:TVOLt:YVALue command.
Example Command Sequence
:MEASure:HORizontal:TEDGe:SOURce CHAN2_2 :MEASure:HORizontal:TEDGe:EDIRection RISing :MEASure:HORizontal:TEDGe:NUMBer 2 :MEASure:HORizontal:TEDGe:THReshold MIDDle :MEASure:HORizontal:TEDGe :MEASure:HORizontal:TEDGe?