:MEASure:HORizontal:TVOLt:YVALue
Command Syntax
:MEASure:HORizontal:TVOLt:YVALue <amplitude>
<amplitude> is a double.
Query Syntax
:MEASure:HORizontal:TVOLt:YVALue?
Description
For the Time-at-Amplitude measurement, specifies the amplitude value at which to perform the measurement. To specify the edge direction, use the :MEASure:HORizontal:TVOLt:EDIRection command. To specify the edge number, use the :MEASure:HORizontal:TVOLt:ENUMber command.
Example Command Sequence
:MEASure:HORizontal:TVOLt:SOURce CHAN1_1 :MEASure:HORizontal:TVOLt:EDIRection RISing :MEASure:HORizontal:TVOLt:ENUMber 1 :MEASure:HORizontal:TVOLt:YVALue 100E-03 :MEASure:HORizontal:TVOLt :MEASure:HORizontal:TVOLt?