:MEASure:HORizontal:TVOLt:REGion
Command Syntax
:MEASure:HORizontal:TVOLt:REGion {DISPlay | WAVeform | REGion{1:8}}
Query Syntax
:MEASure:HORizontal:TVOLt:REGion?
Description
Select a time span over which the :MEASure:HORizontal:TVOLt measurement is made.
- DISPlay
- The measurement is performed on on-screen data only.
- WAVeform
- The measurement is performed on all waveform data, whether the data is displayed on-screen or not.
- REGion{1:8}
- The measurement is performed across one of eight regions. Regions are defined using the
:REGions:REGion{N}:STATecommand.
This setting can affect analysis as waveforms are moved horizontally. For example, a Rise Time measurement is made on the first edge. When DISPlay is selected and a waveform is moved horizontally, as different edges become the first on the screen, the measurement moves to those different edges. When WAVeform is selected, the measurement remains on the first edge in the data even when that edge is moved horizontally off the screen.
Example Command Sequence
:MEASure:HORizontal:TVOLt:SOURce CHAN2_1 :MEASure:HORizontal:TVOLt:REGion REGion3 :MEASure:HORizontal:TVOLt :MEASure:HORizontal:TVOLt?